Перейти к основной информации

Выберите страну/язык

Печать
SCHROFF-CNPT-N01379-KeyVisualQuantumCamp-EN-2404 somenotext 2

nVent SCHROFF New Release Next Generation MTCA.4

nVent SCHROFF New Release Next Generation MTCA.4
  • Revolutionary new MTCA.4 Crate to achieve 128 Gbits bandwidth per slot with PCIe Gen 5

  • Enhanced Cooling:Improved rear card cage cooling

  • Futue Proof: New cooling Unit Manager design based on controller with long life time expectation

  • Downward compatibility: Mix and match legacy and new chassis and cooling units

 

nVent Electric plc (NYSE:NVT) (“nVent”), a global leader in electrical connection and protection solutions, has today announced the launch of its first MTCA.4 Crate in accordance this new released Revision 3.0 of the MTCA.0 standard. It supports PCIe Gen 4/5 and 100 GbE. 

In September 2023 PICMG released the new revision 3.0 of the MTCA.0 specification. This new version adds the support for PCI Express Gen 4 and 5 as well as for 100GBASE-KR4. To accomplish these higher data rates SMD and compression mount connectors have been evaluated by the working group and the simulation results have been taken as a base to define the whole data transmission channel for MicroTCA. The transmission channel has been divided into the logical parts to define the limits for boards and backplane to make sure, all MTCA.0 Rev 3.0 conform MCH’s, AMC’s and Crates work together in a PCI Express Gen4/5 or 100 GbE environment. 

As these high-end switches consume more power compared to the formerly supported ones, the power budget for the MCH, where the switch resides, have been upgraded from 80 W to 110 W. And to make sure that the MCH doesn’t overheat the Cooling Units power budget was also upgraded to 110 W. A software mechanism ensures the downward compatibility of old and new MCH’s, Power Modules and Cooling Units. 

nVent SCHROFF – The most powerful fans in the RTM area within the limits of the newly defined 110W power efficiency.

The Cooling Unit firmware is following the procedure of the revision 3.0 of the MicroTCA specification. When powering up it stays in the 80 W power rating. If the Power Module supports the 110 W per cooling unit channel it will be possible to run all fans at full speed. For Power Modules only supporting 80W or if the IPMI communication gets lost it will stay in the 80W power envelope.

The Renesas H8S controller used successfully on the nVent SCHROFF MTCA.4 Crates has now been set to EOL. This is the reason why nVent SCHROFF now introduces with the new cooling units and additional features described above, a new Cooling unit Manager design based on the STM32 controller from STMicroelectronics.

Providing the highest data bandwidth

To achieve the higher data bandwidth, the maximum trace length defined in MTCA.0 Rev. 3.0 needs to be matched. Therefore, the MCH slots moved from the outside to the middle of the card cage.

17vh4b.png

 

Materials upgraded

The pcb material was changed to a material with lower losses and new SMD connectors are used instead of the press fit ones. For optimized routing the physical order of the AMC modules has been changed. In the past the nVent SCHROFF MTCA.4 Crates used the physical order starting from 1 from left to right, now it’s changed into: 7-8-9-10-11-12-MCH1-MCH2-6-5-4-3-2-1.

О компании nVent

Компания nVent — ведущий мировой поставщик решений для подключения электрических систем и обеспечения их безопасности. Мы считаем, что наши передовые электротехнические решения делают электрические системы более безопасными и, таким образом, способствуют созданию более безопасного мира в целом. Мы проектируем, производим, распространяем, устанавливаем и обслуживаем высокопроизводительное оборудование, а также предлагаем решения в области подключения и обеспечения безопасности для самой чувствительной аппаратуры, сложных зданий и критических процессов. У нас вы найдете обширный ассортимент корпусов, электрических соединителей и фиксаторов, а также решения для терморегуляции. Мы поставляем оборудование ведущим в своих отраслях компаниям, которые ценятся во всем мире за качество, надежность и прогрессивность своих товаров и услуг. Главный офис нашей компании расположен в Лондоне (Великобритания), а офис управления – в Миннеаполисе (США). В нашем портфолио представлены бренды электротехнического оборудования с более чем 100-летней историей, а также такие торговые марки, как nVent CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF и TRACER. Learn more at www.nvent.com

nVent, CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF и TRACER являются торговыми марками, принадлежащими компании nVent Services GmbH или ее аффилированным лицам по праву собственности или на основании лицензии.

Powered by Translations.com GlobalLink Web SoftwarePowered by GlobalLink Web