Перейти к основной информации

Выберите страну/язык

Печать
tradeshow logos 2023

nVent to showcase innovative, modular nVent SCHROFF solutions to safeguard critical communications and electronics systems at Embedded World in March

nVent Electric plc, a global leader in electrical connection and protection solutions, will present innovative solutions at Hall 1, Booth 1-441 during Embedded World from March 14-16, in Nuremberg, Germany. The exhibition will showcase solutions for equipment protection in rugged environments, high-performance computing, cooling and management, and speed and scale. 

At the show, nVent will launch the highly-anticipated nVent SCHROFF Ratiopac-PRO Style modular desktop case portfolio. The new desktop cases provide high-quality protection for electronics components housed in 19” desktop enclosures.The new cases are ideally suited for scientific instrument, optical measurement and visual inspection applications. 
, The new Ratiopac-PRO Style modular desktop case portfolio offers customers the flexibility customize the appearance of each case to reflect their branding and identity. There are thousands of possible configurations to quickly and easily suit customers’ design and protection needs cost-effectively. The new platform includes a wide variety of feature options, including for frames, inlays, panels, colors and other user-driven design elements. 

Featured solutions at the show

See the new modular desktop cases in person as part of the nVent SCHROFF “Products that Protect, Innovations that Inspire” exhibition! 

During Embedded World, nVent will also showcase a wide range of innovative nVent SCHROFF solutions for the test and measurement, aerospace and defense, railway and communications industries. Additional featured nVent SCHROFF solutions will include:
 

  • Enhanced EMC shielding for subracks – As railways rely on more and increasingly powerful electronics, railway applications need stronger protection against the electromagnetic interference that can negatively impact performance and disrupt operations. This is especially important for emerging 5G technologies. The nVent SCHROFF 19” Subracks offer a complete range of protective solutions, including enhanced EMC shielding that increases the effectiveness of radiofrequency (RF) shielding for highly sensitive electronics in harsh environments. Visit the booth to learn more about innovative nVent SCHROFF EMC shielding solutions. 
  • Remote smart hardware management for railway – With the expanding deployment of digital rail, operators need to remotely monitor and control sensitive equipment in the technical control rooms throughout the rail network. Increasingly sophisticated electronic equipment is essential for digital rail operation, which also requires higher levels of control and condition monitoring for remote electronics, smart cooling and sensors. Talk to our product experts about the nVent SCHROFF Remote Smart Hardware Management for Digital Rail solution!
  • Fully equipped testing stand – Choosing the optimal hardware platform for test system design can be a daunting task. The nVent SCHROFF brand provides high-quality racks and enclosures for OEMs and end-users to protect the sensitive electronics that comprise high-end test systems. At the show, a comprehensive solution for automated test equipment will be on display, including the mounted PXIe embedded system, power distribution, climate control and 19” rack. Whatever physical challenges a test system faces, nVent technical experts are ready to collaborate to deliver the best solution.
  • Ruggedized enclosure solutions for small form factors – As systems become smaller and more powerful, they need complete mechanical, electronic, and thermal solutions that can satisfy size, weight and power trends. See an interactive detailed view of a state-of-the-art solution at the show, highlighting the nVent SCHROFF High Thermal Integrated Conduction Cooled Assembly (CCA), which can deliver up to 40 percent improved module thermal resistance over standard CCAs with nVent SCHROFF Card-Lok PCB retainers. Высокотемпературный интегрированный модуль с кондуктивным охлаждением (CCA) идеально подходит для систем VPX как замена традиционным модулям VITA с кондуктивным охлаждением, что позволяет избежать необходимости в проведении серьезной перепроектировки модуля или использования дорогостоящих альтернативных технологий охлаждения. 
  • Discover more nVent SCHROFF solutions that deliver equipment protection in rugged environments, high-performance computing, cooling and management, and speed and scale!

​​​Recognized globally for quality, reliability and innovation to safeguard systems in virtually any environment, the nVent SCHROFF platform – including cabinets, racks, subracks, power distribution, climate control and more – is specially engineered for flexibility. By design, the modular products can be easily and cost-effectively tailored to meet specific application requirements. 

Learn about a full range of nVent SCHROFF products and services, see live demonstrations and talk with trusted nVent experts in Hall 1, Booth 1-441 from March 14-16 at Embedded World.  

Получите свой бесплатный билет прямо сейчас Код регистрации: ew23492706

 

 

О компании nVent 

Компания nVent — ведущий мировой поставщик решений для подключения электрических систем и обеспечения их безопасности. Мы считаем, что наши передовые электротехнические решения делают электрические системы более безопасными и, таким образом, способствуют созданию более безопасного мира в целом. Мы проектируем, производим, распространяем, устанавливаем и обслуживаем высокопроизводительное оборудование, а также предлагаем решения в области подключения и обеспечения безопасности для самой чувствительной аппаратуры, сложных зданий и критических процессов. У нас вы найдете обширный ассортимент корпусов, электрических соединителей и фиксаторов, а также решения для терморегуляции. Мы поставляем оборудование ведущим в своих отраслях компаниям, которые ценятся во всем мире за качество, надежность и прогрессивность своих товаров и услуг. Главный офис нашей компании расположен в Лондоне (Великобритания), а офис управления – в Миннеаполисе (США). В нашем портфолио представлены бренды электротехнического оборудования с более чем 100-летней историей, а также такие торговые марки, как nVent CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF и TRACER. Узнайте больше на веб-сайте www.nvent.com.

nVent, CADDY, ERICO, HOFFMAN, RAYCHEM, SCHROFF и TRACER являются торговыми марками, принадлежащими компании nVent Services GmbH или ее аффилированным лицам по праву собственности или на основании лицензии. 

Get your free ticket and visit us at Booth 1-441 (registration code: ew23492706)

Powered by Translations.com GlobalLink OneLink SoftwarePowered By OneLink